This directive controls the output information and format of the assembler list file. It does not affect code generation.
|
When generating an assembler list file, this directive controls whether to output information to the assembler list file in units of lines from the assembly language file. |
This directive can stop (OFF) outputting lines to the assembler list file.
This directive can stop (OFF) outputting lines to the assembler list file.
Even in the range where line output is stopped, error lines are output to the assembler list file.
This directive can start (ON) outputting lines to the assembler list file.
When this directive is not specified, all lines are output to the assembler list file.
Be sure to insert a space character or a tab between this directive and the operand.