Defines various limits relating to the internal representation of integer type data.
The following macro names are all implementation-defined.
|
|
|
|
|
|
Constant
(macro)
|
CHAR_BIT
|
8
|
Indicates the number of bits in a char type value.
|
|
CHAR_MAX
|
127
|
Indicates the maximum value that can be represented by a char type variable.
|
|
255*1
|
|
CHAR_MIN
|
−128
|
Indicates the minimum value that can be represented by a char type variable.
|
|
0*1
|
|
SCHAR_MAX
|
127
|
Indicates the maximum value that can be represented by a signed char type variable.
|
|
SCHAR_MIN
|
−128
|
Indicates the minimum value that can be represented by a signed char type variable.
|
|
UCHAR_MAX
|
255U
|
Indicates the maximum value that can be represented by an unsigned char type variable.
|
|
SHRT_MAX
|
32767
|
Indicates the maximum value that can be represented by a short type variable.
|
|
SHRT_MIN
|
−32768
|
Indicates the maximum value that can be represented by a short type variable.
|
|
USHRT_MAX
|
65535U
|
Indicates the maximum value that can be represented by an unsigned short type variable.
|
|
INT_MAX
|
217483647
|
Indicates the maximum value that can be represented by an int type variable.
|
|
INT_MIN
|
−2147483647−1
|
Indicates the minimum value that can be represented by an int type variable.
|
|
UINT_MAX
|
4294967295U
|
Indicates the maximum value that can be represented by an unsigned int type variable.
|
|
LONG_MAX
|
217483647L
|
Indicates the maximum value that can be represented by a long type variable.
|
|
LONG_MIN
|
−2147483647L−1L
|
Indicates the minimum value that can be represented by a long type variable.
|
|
ULONG_MAX
|
4294967295U
|
Indicates the maximum value that can be represented by an unsigned long type variable.
|
|
LLONG_MAX
|
9223372036854775807LL
|
Indicates the maximum value that can be represented by a long long type variable.
|
|
LLONG_MIN
|
−9223372036854775807LL
−1LL
|
Indicates the minimum value that can be represented by a long long type variable.
|
|
ULLONG_MAX
|
18446744073709551615ULL
|
Indicates the maximum value that can be represented by an unsigned long long type variable.
|
Notes 1. | Indicates the value that can be represented by a variable when the signed_char option is specified. |