Calculates the arc hyperbolic cosine of a complex number.
float complex cacoshf(float complex z);
double complex cacosh(double complex z);
long double complex cacoshl(long double complex z);
z Complex number for which arc hyperbolic cosine is to be computed
Complex arc hyperbolic cosine of z
The cacoshf function returns the arc hyperbolic cosine in the range [0, π].