Attempts to generate a floating-point exception.
e Value indicating the exception to be generated
When generating an "overflow" or "underflow" floating-point exception, whether the feraiseexcept function also generates an "inexact" floating-point exception is implementation-defined.
Do not use this function when compiler option nofpu is selected. If used, the function returns a nonzero value, which indicates an abnormality.