Everything

wcscat


Concatenates a string after another string.

[Format]

#include <wchar.h>

wchar_t *wcscat(wchar_t *s1, const wchar_t *s2);

[Parameters]

s1 Pointer to the string after which another string is appended

s2 Pointer to the string to be appended after the other string

[Return values]

s1 value

[Remarks]

The wcscat function is the wide-character version of the strcat function.