Everything
Everything
top
Compiler
Usage Notes
11.
Usage Notes
This chapter describes the points to be noted when using the CCRX.
To the latest version of this page
Differences Information
Previous Topic
Standard Library Error Messages
Next Topic
Notes on Program Coding
Table of Contents
GENERAL
COMMAND REFERENCE
OUTPUT FILES
COMPILER LANGUAGE SPECIFICATIONS
ASSEMBLY LANGUAGE SPECIFICATIONS
SECTION SPECIFICATIONS
LIBRARY FUNCTIONAL SPECIFICATION
STARTUP
FUNCTION CALL INTERFACE SPECIFICATIONS
MESSAGES
Usage Notes
Notes on Program Coding
Notes on Compiling a C Program with the C++ Compiler
Notes on Options
Preventing E0562330 Errors in Cases Where Optimization by the Optimizing Linkage Editor is Enabled
Compatibility with an Older Version or Older Revision
W0523041 message [C/C++ compiler]
Using MVTC or POPC instructions [Assembler]
Using the -delete option for linkage [Optimizing linkage editor]
Path names
Usage of math.h functions (frexp, ldex, scalbn and remquo) in C++ language (including EC++)
PIC/PID function (-pic and -pid options)
Eliminated options (for the C/C++ compiler)
C/C++ source-level debugging (for the C/C++ compiler)
Using sections that include address 0xffffffff (in the assembler)
Using -form and -output at the same time (in the linkage editor)
Using function names that begin with _builtin (for the C/C++ compiler)
Function that is specified by #pragma interrupt and for which save_acc is valid has formal parameters [C/C++ compiler]
-merge_files
-cfi_ignore_module
Using fenv.h when -dpfpu is specified
QUICK GUIDE
COPYRIGHT