Everything

2.1 Overview

The resource information tool can be used to confirm the resource information (e.g. system information and memory area information) that changes dynamically as the program executes.
The operating procedures for the resource information tool are described below.
(1) Start CS+
Launch the CS+ from the [start] menu of Windows.
Remark See "CS+ Start" for details on "Start CS+".
(2) Open project
Open the project to debug.
Remark See "CS+ Start" for details on "Open project".
(3) Select debug tool
Select the type of debugging tool with which to debug the program (IECUBE, E1, E20 or Simulator).
Remark See "CS+ RL78 Debug" for details on "Select debug tool".
(4) Download programs
Download the program to debug.
Remark See "CS+ RL78 Debug" for details on "Download programs".
Remarks 1. When a program using the RI78V4 functionality is downloaded, this panel opens automatically.
2. The value will be indeterminate for the resource information shown when the RI78V4 system initialization is incomplete, because it will not be managed by the RI78V4.
(6) Execute/stop programs
Run the program to the location for which you wish to display the resource information.
Remarks 1. See "CS+ RL78 Debug" for details on "Execute/stop programs".
2. You can debug a program efficiently using “Section skip function” of the debugger. For example “step in” execute on a service call issue point, the debugger skip all internal process of RI78V4 and break by reaching the user application part. See "CS+ RL78 Debug" for details on "Section skip function".
Remark
On the Realtime OS Resource Information panel tabs (e.g. [System] tab and [Memory Area] tab), check the current status of the resource information.