Execute the program (see "2.8 Execute Programs").
If the conditions for a Point Trace event that you have set are met while the program is executing, that information is collected as trace data.
See "2.12.6 Display the collected execution history" for details on checking trace data.
![](Debug_RL78_E-276.gif)
![](Debug_RL78_E-277.gif)