By clicking the
button on the toolbar in the Trace panel during program execution, it is possible to temporarily stop collection of trace data without stopping program execution.
Use this function when you want to stop only the trace function without halting the program and check the trace data that has been collected until you stop it.