This timer operation can be configured in the [Trace] category on the [Debug Tool Settings] tab in the Property panel.
Figure 2.88
[Timer] Category [Simulator]
(1)
[Use timer function]
Select whether to use the timer function.
Select [Yes] to use the timer function (default: [No]).