Use the Editor panel shown below to display the source file.
The Editor panel opens automatically after a load module file is successfully downloaded, with the source text at the position you specified (see "2.5.1 Execute downloading") displayed on the panel.
If you want to open the Editor panel manually, double-click on the source file in the Project Tree panel.
For details on the contents and function in each area, see "CS+ Editor".
![](Debug_RX_E-88.gif)