Everything
2.5.1 Output device pin list

Select [File] menu >> [Save Pin List As...] to output a report file (a file containing information configured using Pin Configurator: device pin list).

The destination folder for the device pin list is specified in the Save As dialog box which opens by selecting [File] menu >> [Save Pin List As ...].

Figure 2.12

Output Device Pin List

 

Remark 1.

If a device pin list has been already output, that list will be overwritten by selecting [File] menu >> [Save Pin List].

Remark 2.

The output format for the device pin list is limited to Microsoft Office Excel Book.