This chapter describes the key functions provided by the Code Generator along with operation procedures.
Remark
In this chapter, an example where an RL78/G1E (ROM: 32KB) R5F10FLC(64pin) is the target device is used to explain the key functions.