Everything

PseudoTimerInfo


This class holds pseudo-timer information (return value of debugger.PseudoTimer.Information function). [RL78 instruction simulator]

[Type]

class PseudoTimerInfo:
    Number = None
    VectorAddr = None
    Priority = None
    IntervalTime = None
    IntervalTimeUnit = None
    Periodic = None

[Variable]

Variable

Description

Number

This holds the pseudo-timer number.

VectorAddr

This holds the vector address of the interrupt to be generated when the interval time of the pseudo-timer matches the condition.

Priority

This holds the interrupt priority.

IntervalTime

This holds the interval time of the pseudo-timer.

IntervalTimeUnit

This holds the unit of the interval time.

The following lists the specifiable units.

Type

Description

IntervalTimeUnit.Min

Minutes

IntervalTimeUnit.S

Seconds

IntervalTimeUnit.Ms

Milliseconds

IntervalTimeUnit.Us

Microseconds

IntervalTimeUnit.Ns

Nanoseconds

IntervalTimeUnit.Clock

CPU clock cycles

Periodic

This holds whether an interrupt is to be generated each time the specified time elapses.

True: An interrupt is generated each time the specified interval elapses.

False: An interrupt is only generated once.

[Detailed description]

-

PseudoTimerInfo is a class, and it is passed as the return value when the debugger.PseudoTimer.Information function is executed.