This class holds information on the save register bank (return value of the debugger.SaveRegisterBank.Information function). [RX]
[Type]
class BankedRegisterInfo:
BankNumber = ""
RegisterName = ""
Value = ""
|
[Variable]
|
|
|
|
BankNumber
|
This holds the bank number.
|
|
RegisterName
|
This holds the name of the register.
|
|
Value
|
This holds the value.
|
[Detailed description]
[Example of use]
>>> srb = debugger.SaveRegisterBank.Information([1, 3])
Save register bank 1
R1 0x00000000
R2 0x00000000
...
ACC0 0x000000000000000000
ACC1 0x000000000000000000
Save register bank 3
R1 0x00000000
R2 0x00000000
...
ACC0 0x000000000000000000
ACC1 0x000000000000000000
--------------
>>> print srb[0].BankNumber
1
>>> print srb[0].RegisterName
R1
>>> print srb[0].Value
0
|