This function displays the string on the Output panel.
[Specification format]
common.OutputPanel(output, messageType = MessageType.Information)
|
[Argument(s)]
|
|
|
|
output
|
Specify the string displayed on the Output panel.
|
|
messageType
|
Specify the type of messages to be colored in the Output panel.
The colors are in accord with the settings for the [General - Font and Color] category in the Option dialog box.
|
|
|
|
|
MessageType.Error
|
Error
|
|
MessageType.Information
|
Standard (default).
|
|
MessageType.Warning
|
Warning
|
[Return value]
If the string was displayed on the Output panel successfully: True
If there was an error when displaying the string on the Output panel: False
[Detailed description]
- | This function displays the string specified by output on the Output panel. |
[Example of use]
>>>common.OutputPanel("An error occurred.", MessageType.Error)
True
>>>
|