Everything

debugger.RecoverSWAS


This function recovers the Switch Area Status. [RH850G4MH, RH850G4KH] [E2/E2 Lite/IE850A]

[Specification format]

debugger.Register.RecoverSWAS()

[Argument(s)]

None

[Return value]

If recovery of the Switch Area Status was successful : True

If recovery of the Switch Area Status failed : False

[Detailed description]

-

This function recovers the Switch Area Status.

[Example of use]

>>>debugger.RecoverSWAS()
True
>>>