Everything

debugger.PseudoTimer.Delete


This function deletes pseudo-timers. [RL78 instruction simulator]

[Specification format]

debugger.PseudoTimer.Delete(pseudoTimerNumber = 0)

[Argument(s)]

Argument

Description

pseudoTimerNumber

Specify the pseudo-timer number to be deleted (numerical value: 1 to 64).

Delete all pseudo-timers (numerical value: 0).

[Return value]

If pseudo-timers were deleted successfully :True

If there was an error when deleting pseudo-timers:False

[Detailed description]

-

This function stops and deletes pseudo-timers specified with pseudoTimerNumber.

-

If pseudoTimerNumber is not specified or is specified as 0, pseudo-timers with all pseudo-timer numbers will be stopped and deleted.

[Example of use]

>>>debugger.PseudoTimer.Delete(1)
True
>>>debugger.PseudoTimer.Delete()
True