This function opens a project.
[Specification format]
project.Open(fileName, save = False)
|
[Argument(s)]
|
|
|
|
fileName
|
Specify a project file.
|
|
save
|
If another project was opened, specify whether to save any files being edited and the project when you close it.
True: Save all editing files and a project.
False: Do not save all editing files and a project (default).
|
[Return value]
If the project was closed successfully: True
If there was an error when closing the project: False
[Detailed description]
- | This function opens a project specified by fileName. |
- | If other project is opened, that project is closed.
If save is set to "True", then all files being edited and a project are saved. |
- | If other project is not opened, the setting of save is ignored. |
[Example of use]
>>>project.Open(r"C:/test/test.mtpj")
True
>>>
|