This function runs a build.
[Specification format]
build.All(rebuild = False, waitBuild = True)
|
[Argument(s)]
|
|
|
|
rebuild
|
Specify whether to run a rebuild of a project.
True: Run a rebuild of a project.
False: Run a build of a project (default).
|
|
waitBuild
|
Specify whether to wait until completing a build.
True: Wait until completing a build (default).
False: Return a prompt without waiting to complete a build.
|
[Return value]
- | When waitBuild is set to "True" |
If a build was completed successfully: True
If a build failed or was canceled: False
- | When waitBuild is set to "False" |
If a build successfully started execution: True
If a build failed to start execution: False
[Detailed description]
- | This function runs a build of a project.
If a subproject is added to the project, a build of the subproject is run. |
- | If rebuild is set to "True", then a rebuild of a project is run. |
- | If waitBuild is set to "False", then a prompt is returned without waiting to complete a build. |
- | Regardless of whether a build is successful, the build.BuildCompleted event is issued when a build completes. |
[Example of use]