|
|
|
|
The package is not correctly installed, or a required file has been deleted.
|
|
Please reinstall the real-time OS package.
|
|
|
Cannot connect to the debugger.
|
|
Cannot communicate with debugger for unknown reason.
|
|
Please contact your vendor or Renesas Electronics.
|
|
|
|
|
The target program is not loaded in the debugger, or there is no real-time OS incorporated in the target program.
|
|
Load the target program into the debugger. If there is no real-time OS incorporated in the target program, do so.
|
|
|
RTOS data may be corrupted.
|
|
The real-time OS information is incorrect (e.g. runaway program).
|
|
Make sure that the real-time OS information of the target program is not corrupt.
|
|
|
Queue information may be corrupted.
|
|
The real-time OS information is incorrect (e.g. runaway program).
|
|
Make sure that the real-time OS information of the target program is not corrupt.
|
|
|
Realtime OS used in the project is not installed.
|
|
The real-time OS used by the existing project was not found (for example, it may have been uninstalled).
|
|
Make sure that the real-time OS is correctly installed.
|
|
|
RI850MP supports the 32 register mode only.
|
|
Displayed when the register mode of the project that uses RI850MP is changed besides 32-register mode.
|
|
Set the register mode to 32-register mode.
|
|
|
Saving realtime OS build setting options failed.
|
|
Could not obtain save information because the internal information is corrupt.
|
|
Create the project again, or re-install the plug-in.
|
|
|
Illegal keyword or syntax error.
|
|
The keyword is illegal or there is a description error.
|
|
Check the description format of the system configuration file or command file.
|
|
|
Keyword ( xxx) is too longer than 24 characters.
|
|
The keyword ( xxx) is longer than the maximum value of 24 characters permitted for that keyword.
|
|
Specify a keyword (object name) of 24 characters or less.
|
|
[RI78V4 V2 .xx.xx] [RI850V4 V1 .xx.xx] [RI850V4 V2 .xx.xx]
Keyword ( xxx) is too longer than 255 characters.
|
|
[RI78V4 V2 .xx.xx] [RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
The keyword ( xxx) is longer than the maximum value of 255 characters permitted for that keyword.
|
|
[RI78V4 V2 .xx.xx] [RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Specify a keyword ( xxx) of 255 characters or less.
|
|
Keyword ( xxx) is too longer than ( yyy) characters.
|
|
Specify a keyword ( xxx) of yyy characters or less.
|
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
The specified numeric value is too large to be processed within CF78V4.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
Specify a numeric value within the 32-bit data range.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
The specified numeric value is too large to be processed within CF850V4.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Specify a numeric value within the 32-bit data range.
|
|
|
Keyword ( xxx) is not defined.
|
|
Check the definition of the keyword.
|
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Memory area ( xxx) cannot be specified for system stack.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Specify the memory area that can be specified.
|
|
Memory area ( xxx) cannot be specified for system stack.
|
|
Review the format of system stack information SYS_STK.
|
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Revise the number of characters of each item and do 1 line within 16384 character.
|
|
|
Keyword ( xxx) is already defined.
|
|
The keyword ( xxx) is already defined.
|
|
Define a keyword only once.
|
|
|
Keyword ( xxx) cannot be defined in DOMAIN.
|
|
|
Keyword ( xxx) cannot be defined out of DOMAIN.
|
|
|
DOMAIN allocation is defined more than defined DOMAIN.
|
|
|
DOMAIN allocation is defined less than defined DOMAIN.
|
|
|
Number of PE is not defined.
|
|
|
Task is not defined on any DOMAIN.
|
|
|
|
|
|
Too many Keyword ( xxx) is defined.
|
|
There are too many definitions of keyword ( xxx).
|
|
Decrease the number of definitions of keyword so as not to exceed the maximum.
|
|
|
Too few Keyword ( xxx) is defined.
|
|
|
Task ( xxx) that is specified in task exception routine is undefined.
|
|
Make sure whether a specified task exists.
|
|
|
Task exception routine for the one task is multiple defined ( xxx).
|
|
Check the definition of the corresponding task exception routine.
|
|
|
Illegal maximum value ( xxx).
|
|
Check the specified value.
|
|
|
Illegal exception code ( xxx).
|
|
Check the specified exception code.
|
|
|
Exception code ( xxx) is out of range.
|
|
Check the specified exception code.
|
|
|
Number of maximum handler is out of range ( xxx).
|
|
Check the number of interrupt handlers.
|
|
|
Undefined Memory area ( xxx).
|
|
Check the definition of memory area.
|
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
One of TA_HLNG or TA_ASM must be defined as attribute in xxx.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
Specify either TA_HLNG or TA_ASM.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
One of TA_HLNG or TA_ASM must be defined as attribute in Keyword ( xxx).
|
|
|
Attribute ( yyy) is not defined together in Keyword ( xxx).
|
|
Specify either xxx or yyy.
|
|
|
One of TA_TFIFO or TA_TPRI must be defined as attribute in Keyword (CRE_MTX).
|
|
Specify either TA_TFIFO or TA_TPRI.
|
|
|
One of TA_MFIFO or TA_MPRI must be defined as attribute in xxx.
|
|
Specify either TA_MFIFO or TA_MPRI.
|
|
|
Neither TA_INHERIT and TA_CEILING may not be specified in this version.
|
|
|
|
|
Total memory size ( xxx) that is allocated in the memory area ( yyy) exceeds defined size ( zzz).
|
|
Reduce the total size of the memory area ( yyy) so as not to exceed the maximum size.
|
|
|
Start address ( xxx) is not 2 bytes alignment.
|
|
|
|
|
Illegal memory area ( xxx).
|
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
xxx( yyy) bigger than maximum 255 was set.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx]
Check the value of keyword.
|
|
xxx ( yyy) bigger than maximum ( zzz) was set.
|
|
Check the value of keyword.
|
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
cyctim ( xxx) smaller than minimum ( yyy) was set.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
For the activation cycle for the cyclic handler, specify a value from 1 to 4294967295 (0xffffffff).
|
|
xxx ( yyy) smaller than minimum ( zzz) was set.
|
|
|
Memory area size of fixed-sized memory pool (= block count ( xxx) *block size ( yyy) ) is out of range.
|
|
Specify the memory block count and block size so that the memory area size of the fixed-sized memory pool (calculation result of memory block count x block size) will fall within the range of 4 to 65534 (0xfffe).
|
|
|
Attribute ( xxx) is not supported.
|
|
Check a specifiable attribute.
|
|
|
Attribute ( xxx) is not defined ( yyy).
|
|
Check the attribute and then specify xxx.
|
|
|
xxx ( yyy) is out of range.
|
|
|
|
|
|
|
|
|
|
Illegal OS version ( xxx).
|
|
|
|
|
The number of lines exceeded the maximum.
|
|
Set the number of lines of the file to no more than 1000000 lines.
|
|
|
Stack check flag is illegal.
|
|
Check the specified stack check flag.
|
|
|
Illegal system stack size( xxx)
|
|
Set the system stack size to a value from 0 to 65534 (0xfffe).
|
|
|
Illegal maximum task priority ( xxx).
|
|
Set the value of maximum task priority information (MAX_PRI) to a value from 1 to 15.
|
|
|
Exception code for system timer ( xxx) is out of range.
|
|
Check the exception code for system timer.
|
|
|
Number of maximum interrupt factor is out of range ( xxx).
|
|
Check the number of maximum interrupt factor.
|
|
|
Cyclic time of system time is illegal ( xxx).
|
|
Check the specified value at cyclic time.
|
|
|
Task extension information is out of range ( exinf).
|
|
Specify a value from 0x0 to 0xfffff for the task extension information (ext_inf).
|
|
|
Function address ( xxx) is out of range.
|
|
|
Task stack size is out of range ( xxx).
|
|
Set the task stack size to a value from 0 to 65534 (0xfffe).
|
|
|
Initial semaphore number ( xxx) is out of range.
|
|
Set the number of initial resources for semaphore to a value from 0 to 127.
|
|
|
Block size ( xxx) of fixed-sized memory pool is out of range.
|
|
Specify a value from 4 to 65534 (0xfffe) for the block size of the fixed-sized memory pool.
|
|
|
Block count ( xxx) of fixed-sized memory pool is out of range.
|
|
Specify a value from 1 to 16383 (0x3fff) for the memory block count of the fixed-sized memory pool.
|
|
|
The interrupt source name ( xxx) is not defined in the device file.
|
|
Check the specified value at cyclic time.
|
|
|
|
|
Check the specifiable range of values.
|
|
|
Name ( xxx) is already used in Keyword ( xxx).
|
|
Check the specified keyword.
|
|
|
Exception code is reserved ( xxx).
|
|
|
Memory area ( xxx) is already defined.
|
|
Check the specified memory area.
|
|
|
Name ( xxx) is already used.
|
|
Specify an object name that is not in use.
|
|
|
Symbol too long (max 30).
Symbol too long (max 4095).
|
|
The symbol name or object name is longer than the maximum value of 30 characters permitted for those names.
The symbol name or object name is longer than the maximum value of 4095 characters permitted for those names.
|
|
Specify a symbol name or object name of 30 characters or less.
Specify a symbol name or object name of 4095 characters or less.
|
|
|
Symbol ( xxx) is already used.
|
|
The symbol name ( xxx) is already defined.
|
|
Specify a symbol name that is not in use.
|
|
|
Address ( xxx) is out of range.
|
|
The specified address ( xxx) is outside the specifiable range.
|
|
Set the address value to a value from 0x0 to 0xfffff.
|
|
|
|
|
Check the specifiable range of values.
|
|
|
DOMAIN name ( xxx) is not defined.
|
|
|
DOMAIN with a PE ( xxx) is not defined.
|
|
|
SYS_STK necessary to a PE ( xxx) is not defined.
|
|
|
Task priority ( xxx) is higher than max priority ( yyy).
|
|
Check the specified task priority.
|
|
|
[RI78V4 V1 .xx.xx] [RI78V4 V2 .xx.xx]
Task priority ( xxx) is higher than the highest system priority 15.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
The specified initial task priority (pri) is higher than the highest system priority 15.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
Set the value of the initial task priority to a value from 1 to 15.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx] [RI850MP]
Task priority ( xxx) is higher than the highest system priority ( yyy).
|
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
Task priority ( xxx) is lower than the lowest system priority 1.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
The specified initial task priority ( xxx) is lower than the lowest system priority 1.
|
|
[RI78V4 V1. xx.xx] [RI78V4 V2. xx.xx]
Set the value of the initial task priority ( xxx) to a value from 1 to 15.
|
|
[RI850V4 V1. xx.xx] [RI850V4 V2. xx.xx] [RI850MP]
Task priority ( xxx) is lower than the lowest system priority ( yyy).
|
|
|
Initial semaphore number ( xxx) is bigger than maximum semaphore number ( yyy).
|
|
Check the specified initial semaphore number.
|
|
|
The interrupt source name ( xxx) cannot be used when not defined in the device file (not set -cpu option).
|
|
Check the specified device file or exception factor.
|
|
|
Handlers that has same exception code in the same PE cannot be defined.
|
|
Check the specified exception factor.
|
|
|
Handlers that has same exception code ( xxx) in the system cannot be defined.
|
|
|
SVC Handlers that has same function code ( xxx) in the system cannot be defined.
|
|
Check the specified function code.
|
|
|
The Number of interrupt handler(%d) is bigger than the number of interrupt factor(%d).
|
|
Check the specified function code.
|
|
|
The exception code that is out of range is already defined.
|
|
Check the specified function code.
|
|
|
The file filename does not exist.
|
|
Specify a correct file name.
|
|
|
Reading analysis data failed. The file type is invalid.
|
|
The format specified for the file is incorrect or the file may have been corrupted.
|
|
Specify the correct format for the file containing the results of analysis and read it again.
|
|
|
Could not operate the hardware trace method. Check whether the debugging tool has a trace function.
|
|
Check whether the debugging tool has a trace function.
|
|
|
Could not switch the trace of task analyzer on. The point trace is full.
|
|
When using the debug tool to specify an event, invalidate or delete the point trace.
|
|
|
Could not find the target to jump.
|
|
Symbol information was not included.
|
|
Use a load module which has symbol information.
|
|
|
|
|
The input value includes illegal characters.
|
|
Specify characters for which input is allowed.
|
|
|
The value is out of range.
|
|
The input value exceeds the range of values that can be input.
|
|
Check the range of values that can be input.
|
|
|
|
|
|
|
|
|
|
The setting for definition name xxx is illegal.
|
|
yyy specified in xxx is invalid. Please revise.
|
|
|
|
|
The specified strings xxx cannot be recognized as a definition name.
|
|
Correct the definition name for xxx.
|
|
|
|
The specified strings yyy as xxx cannot be recognized as a kerword.
|
|
Correct the kerword for yyy.
|
|
|
xxx's ID number is too large. --> < yyy>
|
|
ID number yyy specified in xxx[] is too large.
|
|
The ID number must be no greater than the number of objects that have been defined.
|
|
|
Task[ xxx]'s priority is too large. --> < yyy>
|
|
task[ xxx].priority setting yyy is greater than system.priority.
|
|
Set task[].priority to a value no greater than system.priority.
|
|
|
clock.IPL is too large.--> < xxx>
|
|
The clock.IPL setting is greater than the system.system_IPL setting.
|
|
Set clock.IPL to a value no greater than system.system_IPL.
|
|
|
System timer's vector < xxx> conflict
|
|
A interrupt_vector[ xxx] has already defined for the CMT's vector when one of CMT0, CMT1, CMT2, or CMT3 is specified for clock.timer.
|
|
Delete the interrupt_vector[], or change the clock.timer setting.
|
|
|
< xxx> is already defined.
|
|
|
|
|
|
|
xxx[ yyy] is already defined.
|
|
The ID number is multiply defined in yyy object xxx.
|
|
Ensure that ID numbers do not overlap.
|
|
|
|
|
Zero division expression.
|
|
|
|
|
Can't specify F switch when os_int=YES.
|
|
You cannot specify fast interrupts (pragma_switch=F) for the kernel interrupt handler (os_int=YES).
|
|
Do not set the pragma_switch to F for kernel interrupts.
Set to a non-kernel interrupt (os_int=NO) for fast interrupts.
|
|
|
interrupt_vector[ xxx].os_int must be YES.
|
|
Relocatable interrupt cannot be used as non-kernel interrupt (os_int=NO) when the kernel interrupt mask level (system.system_IPL) is 15.
|
|
Set os_int=YES for all variable vector definitions (interrupt_vector[]).
|
|
|
mailbox[ xxx].max_pri( yyy) is bigger than system.message_pri( zzz).
|
|
The mailbox[ xxx].max_pri setting yyy is greater than the system.message_pri setting zzz.
|
|
Specify a value for mailbox[].max_pri that is no greater than system.message_pri.
|
|
|
Neither system.tic_nume nor system.tic_deno is 1.
|
|
Set 1 to either system.tic_nume or tic_deno as CCC at least.
|
|
|
Symbols other than NO and NO are defined simultaneously.
|
|
You cannot specify symbols other than NO and NO simultaneously.
|
|
|
semaphore[ xxx].initial_count is bigger than semaphore[ xxx].max_count
|
|
The initial_count setting in semaphore[ xxx] is greater than the max_count setting.
|
|
Set initial_count to no greater than max_count.
|
|
|
Size of memorypool[ xxx] is larger than VTMAX_AREASIZE
|
|
The size of fixed-sized memory pool must be lower than or equal to VTMAX_AREASIZE (256MB).
|
|
Set the value of memorypool[ xxx].siz_block * meorypool[ xxx].num_block to no greater than 256 MB.
|
|
|
variable_memorypool[ xxx].max_memsize is larger than 192MB-12
|
|
variable_memorypool.max_memsize must be lower than or equal to "192MB - 12".
|
|
Set variable_memorypool[ xxx].max_memsize to no more than 192 MB - 12.
|
|
|
mutex[ xxx].ceilpri is bigger than system.priority.
|
|
mutex.ceilpri must be lower than or equal to system.priority.
|
|
Set mutex[].ceilpri to no greater than system.priority.
|
|
|
xxx is not a multiple of y.
|
|
xxx must be multiple of y.
|
|
Set xxx to a multiple of y.
|
|
|
max_msgsz ( xxx) is larger than mbf_size( yyy) - 4 .
|
|
The setting of xxx for message_buffer[].max_msgsz exceeds the message_buffer[].mbf_size - 4 setting of yyy - 4.
|
|
Set message_buffer[].max_msgsz to no greater than message_buffer[].mbf_size - 4.
|
|
|
variable_memorypool[ xxx].max_memsize( yyy) is too large. (Max.= zzz)
|
|
The value yyy specified for variable_memorypool[xxx].max_memsize is too large. The maximum value of the specified pool size (variable_memorypool[].heap_size) is zzz.
|
|
Set max_memsize to no more than zzz.
|
|
|
|
|
The base clock cycle time decided by system.tic_nume and system.tic_deno is too long.
|
|
Make the base clock cycle time shorter, or lower clock.timer_clock.
|
|
|
|
|
The base clock cycle time decided by system.tic_nume and system.tic_deno is too short.
|
|
Make the base clock cycle time longer, or higher clock.timer_clock.
|
|
|
cyclic_handler.phs_counter is larger than interval_counter.
|
|
Set cyclic_hand.phs_counter to no greater than interval_counter.
|
|
|
start_address must be smaller than end_address.
|
|
When numeric value is specified as both memory_object.start_addrsss and endaddress, set start_address and end_address that it satisfies the fomula "start_address < and_address".
|
|
|
ACC and NOACC can't be specified at the same time.
|
|
Do not specify both ACC and NOACC at the same time.
|
|
|
task[ xxx].domain_num(= yyy) is bigger than maxdefine.max_domain(= zzz).
|
|
The setting of yyy for task[ xxx].domain_num exceeds the maxdefine.max_domain setting of zzz.
|
|
Set ask[ xxx].domain_num to no greater than maxdefine.max_domain.
|
|
|
|
|
There is not enough memory to execute cfg600 or cfg600px.
|
|
Please contact your vendor or Renesas Electronics.
|
|
|
Illegal argument --> < xxx>
|
|
Failed to recognize xxx due to error in startup format.
|
|
Check the startup format.
|
|
|
|
|
The file " xxx" cannot be generated.
|
|
Check the read-only attribute of the cfg600 or cfg600px output directory and output file.
|
|
|
|
|
The file cannot be accessed in the directory indicated by environment variable "LIB600".
|
|
Make sure that the environment variable "LIB600" setting and directory pointed to by LIB600 are correct.
|
|
|
|
|
The version file cannot be found in the current directory or the directory indicated by environment variable "LIB600".
|
|
Make sure that the environment variable "LIB600" setting and directory pointed to by LIB600 are correct.
|
|
|
Can't open default configuration file.
|
|
The default.cfg file cannot be found in the current directory or the directory indicated by environment variable "LIB600".
|
|
Make sure that the environment variable "LIB600" setting and directory pointed to by LIB600 are correct.
|
|
|
Can't open configuration file < xxx>
|
|
The specified system configuration file " xxx" cannot be accessed.
|
|
Check for the system configuration file settings.
|
|
|
|
|
(2) The definition of the object of the displayed number leaks. This error occurs with O1004 (E).
|
|
(2) Correct the ID number that caused error 01004 (E).
|
|
|
|
|
|
|
|
|
|
|
Initial start task is not defined.
|
|
There is no task[ ] definition with task[].initial_start=ON.
|
|
Define at least one task specified as "ON" in task[].initial_start.
|
|
|
Environment variable "LIB600" not prepared.
|
|
Environment variable LIB600 is not defined.
|
|
Set environment variable "LIB600".
|
|
|
memory_object is not defined.
|
|
Any memory object is not defined.
|
|
Define at least one memory object.
|