This tab shows the detailed information on each file categorized by the following and the configuration can be changed.
 
(1)  [File Information]
(2)  [Notes]
[Description of each category]
The detailed information on the file is displayed and the configuration can be changed.
| 
 
File name 
 | 
 
The file name is displayed. 
Change the file name on the project tree. 
 | 
| 
 
Default 
 | 
 
file name 
 | 
| 
 
How to change 
 | 
 
Changes not allowed 
 | 
| 
 
Relative path 
 | 
 
The relative path from the project folder is displayed. 
 | 
| 
 
Default 
 | 
 
The relative path from the project folder 
 | 
| 
 
How to change 
 | 
 
Changes not allowed 
 | 
| 
 
Absolute path 
 | 
 
The absolute path of the file is displayed. 
 | 
| 
 
Default 
 | 
 
The absolute path of the file 
 | 
| 
 
How to change 
 | 
 
Changes not allowed 
 | 
| 
 
Save with absolute path 
 | 
 
Select whether to save the file location with the absolute path. 
This property is not displayed if the Property panel being displayed while a dependency file is selected on the project tree. 
 | 
| 
 
Default 
 | 
 
No 
 | 
| 
 
How to change 
 | 
 
Select from the drop-down list. 
 | 
| 
 
Restriction 
 | 
 
Yes 
 | 
 
Saves the file location with the absolute path. 
 | 
| 
 
No 
 | 
 
Saves the file location with the relative path. 
 | 
| 
 
Last update 
 | 
 
The time and date on which this file was changed last is displayed. 
 | 
| 
 
Default 
 | 
 
File updated time and date 
 | 
| 
 
How to change 
 | 
 
Changes not allowed 
 | 
| 
 
Writable 
 | 
 
Select whether to enable writing to the file. 
This property is not displayed if the Property panel being displayed while a dependency file is selected on the project tree. 
 | 
| 
 
Default 
 | 
 
Yes (when the file is write enabled) 
No (when the file is not write enabled) 
 | 
| 
 
How to change 
 | 
 
Select from the drop-down list. 
 | 
| 
 
Restriction 
 | 
 
Yes 
 | 
 
Enables the file to write. 
 | 
| 
 
No 
 | 
 
Does not enable the file to write. 
 | 
 
The detailed information on notes is displayed and the configuration can be changed.
This category is not displayed if the Property panel being displayed while a dependency file is selected on the project tree.
| 
 
Memo 
 | 
 
Add memos to the file. 
Add one item in one line. 
The specified memo is displayed as the subproperty. 
 | 
| 
 
Default 
 | 
 
Memo[number of items] 
 | 
| 
 
How to change 
 | 
 
Edit by the Text Edit dialog box which appears when clicking the [...] button. 
For the subproperty, you can enter directly in the text box. 
 | 
| 
 
Restriction 
 | 
 
Up to 256 characters 
Up to 256 items can be specified. 
 |