You can remove the specific file from the build target out of all the files added to the project.
Select the file to be removed from the build target on the project tree and select the [Build Settings] tab on the Property panel.
Select [No] on the [Set as build-target] property in the [Build] category.