2.4.5  
Change the project name
 
You can change the name of the project (main project or subproject) on the project tree.
Select the Project node or Subproject node and select [Rename] on the context menu.
Figure 2.22  | [Rename] Item (For a Project)  | 
 
 
Remark  | After changing the project name, when you save the project, the actual name of the project file is also changed.  |