Everything
2.10.6 Information set for each user of the PC

The common information between projects such as that specified in the Option dialog box is saved in the information file set for each user of the PC (c1_user.mtpu).

 

Type of CS+

Location where the information file set for each user of the PC is stored

CS+ installed with the use of the installer

C:\Users\<user name>\AppData\Local\Renesas Electronics CS+\c1_user.mtpu

CS+ not installed with the use of the installer

<same folder as that for CubeSuiteW+.exe>\UserSettingFolder\<user name>\c1_user.mtpu