The following initial settings are required to use a floating license.
In the License Manager window, click the [Option] button
![](LicenseManager_Eng-22.gif)
The License Manager Option dialog box will open.
Enter the IP address (example: 192.168.0.1) or host name (example: license.example.com) of the license server into [Server Address], the port number specified by the license server administrator into [Port]. If you don’t know, please contact the license server administrator.
![](LicenseManager_Eng-23.gif)
When connection to the license server is successful, the display changes to that shown on the below.
![](LicenseManager_Eng-24.gif)