Everything
2.8 Setting up the Floating License

The following initial settings are required to use a floating license.

Caution

Set up the client after the server settings were finished.

(1)

Open the License Manager Option dialog box

In the License Manager window, click on the [Option] button.

Figure 2.9

License Manger Window

 

The License Manager Option dialog box will open.

(2)

Connect the license server

Enter the IP address (example: 192.168.0.1) or host name (example: license.example.com) of the license server into [Server Address] and the port number specified by the license server administrator into [Port]. If you do not know, please contact the license server administrator.

 

Click on the [Enable] button.

Figure 2.10

License Manager Option Dialog Box (Disabled)

 

When connection to the license server is successful, the display changes to that shown on the below.

Figure 2.11

License Manager Option Dialog Box (Enabled)

 

Click on the [OK] button to close the dialog box.