#include "r_cg_macrodriver.h" #include "r_cg_rtc.h" MD_STATUS R_RTC_Get_CounterValue ( rtc_counter_value_t * const counter_read_val );  | 
カウント値rtc_counter_value_tについての詳細は,R_RTC_Set_CounterValueを参照してください。  | 
MD_BUSY1,またはMD_BUSY2が返却される場合は,カウンタの動作が停止している,またはカウンタの動作開始待ち時間が短いことに起因している可能性があるため,ヘッダ・ファイルr_cg_rtc.hで定義されているマクロ_RTC_WAITTIMEの値を大きくしてください。  |