-show=xreferenceオプションを指定した場合,シンボルの参照情報(クロス・リファレンス情報)を出力します。
*** Cross Reference List *** (1) (2) (3) (4) (5) No Unit Name Global.Symbol Location External Information 0001 sample1 SECTION=.text _main 00000000 _func_01 00000018 SECTION=.data _gval3 fe600000 0003(00000032:.text) 0003(00000038:.text) SECTION=.bss _gval1 fe600004 0001(0000001a:.text) 0001(00000020:.text) _gval2 fe600008 0002(00000026:.text) 0002(0000002c:.text) 0002 sample2 SECTION=.text _func02 00000024 0001(0000000a:.text) 0003 sample3 SECTION=.text _func03 00000030 0001(00000010:.text) |