3.2.10 16-bit timer KB

Below is a list of API functions output by the Code Generator for 16-bit timer KB use.

Table 3.10

API Functions: [16-bit Timers KB]

API Function Name

Function

R_TMR_KB_Create

Performs initialization necessary to control the 16-bit timer KB.

R_TMR_KBm_Create_UserInit

Performs user-defined initialization relating to the 16-bit timer KB.

r_tmr_kbm_interrupt

Performs processing in response to the timer interrupt.

R_TMR_KBm_Start

Starts the count for 16-bit timer KB.

R_TMR_KBm_Stop

Ends the count for 16-bit timer KB.

R_TMR_KBm_Set_PowerOff

Halts the clock supplied to the 16-bit timer KB.

R_TMR_KBmn_ForcedOutput_Start

Enables input of the trigger signal used for the forced output stop function.

R_TMR_KBmn_ForcedOutput_Stop

Disables input of the trigger signal used for the forced output stop function.

R_TMR_KBm_BatchOverwriteRequestOn

Enables batch overwriting of the compare register.