3.2 Function Reference

This section describes the API functions output by the Code Generator, using the following notation format.

Figure 3.1

Notation Format of API Functions

(1)

Name

Indicates the name of the API function.

(2)

Outline

Outlines the functions of the API function.

(3)

[Syntax]

Indicates the format to be used when describing an API function to be called in C language.

(4)

[Argument(s)]

API function arguments are explained in the following format.

I/O

Argument

Description

(a)

(b)

(c)

(a)

I/O

Argument classification

I ... Input argument

O ... Output argument

(b)

Argument

Argument data type

(c)

Description

Description of argument

(5)

[Return value]

API function return value is explained in the following format.

Macro

Description

(a)

(b)

(a)

Macro

Macro of return value

(b)

Description

Description of return value