Add Folder and File dialog box


This dialog box is used to add existing files and folder hierarchies to the project.

The folder is added as a category.

Figure A.10

Add Folder and File Dialog Box

 

The following items are explained here.

[How to open]

-

Drag the folder from Explorer or the like, and drop it on the Project Tree panel.

[Description of each area]

(1)

[File type] area

Select the type of the file to be added to the project.

You can select multiple file types by left clicking while holding down the [Ctrl] or [Shift] key.

If nothing is selected, it is assumed that all types are selected.

(2)

[Subfolder level to search] area

Directly enter the number of levels of the subfolder to be added to the project.

"1" is displayed by default.

Remark

Up to 10 (decimal number) can be specified.
When the input violates any restriction, the following messages will be shown in the tooltip.

Message

Description

Fewer than 0 or more than 10 values cannot be specified.

More than 10 subfolder levels have been specified.

Specify in decimal.

A number in other than decimal or a string has been specified.

[Function buttons]

Button

Function

OK

Adds the folder that was dragged and dropped and the files in that folder to the project. And then closes this dialog box.

Cancel

Does not add the folder and files, and then closes this dialog box.

Help

Displays the help of this dialog box.