A.1 Description

Below is a list of the windows, panels, and dialog boxes related to the basic operations of CS+ and the procedure of build using CS+.

Table A.1

Window/Panel/Dialog Box List

Window/Panel/Dialog Box Name

Function Description

Main window

This is the start-up window that opens when CS+ is launched.

Start panel

This panel allows you to easily open a tutorial, access (create/open) a project, or load a sample project.

Create Project dialog box

This dialog box is used to create new projects or subprojects.

Source Convert Setting dialog box [CC-RL]

This dialog box configures the composition files of the source project (the source files and the like) to convert them for the build tool of the project to be created.

Project Convert Setting dialog box

This dialog box includes the settings for conversion from e2 studio and the old development environment (CubeSuite, HEW, PM+) project (or workspace) to a CS+ project.

Project Tree panel

This panel is used to display components of the microcontroller, build tool, and source file of the project in tree view.

Change Microcontroller dialog box

This dialog box is used to change the microcontroller to be used in the project.

Add File dialog box

This dialog box is used to create a new file and add it to the project.

Add Folder and File dialog box

This dialog box is used to add existing files and folder hierarchies to the project.

Property panel

In this panel, the detailed information on the node that is selected in the Project Tree panel is displayed categorized. Also, the settings of the selected node can be changed.

Character String Input dialog box

This dialog box is used to input and edit characters in one line.

Text Edit dialog box

This dialog box is used to input and edit texts in multiple lines.

Path Edit dialog box

This dialog box is used to edit or add the path or file name including the path.

Smart Browser panel

This panel is used to list various documents (user's manuals, technical updates, application notes, and tool news) related to the device selected for the active project and allow downloading of sample code, if any, that comes with the applicable application notes.

Output panel

This panel is used to display the message that is output from the build tool/debug tool/each plug-in or the result of the Find In Files with the Find and Replace dialog box.

Error List panel

This panel is used to list the information of messages output from the build tool (error information).

Memory Mapping Profiler panel

This panel is used to display the memory mapping information of load modules collected by the build tool.

The amount of used memory can be reduced by analyzing the information.

Column Chooser dialog box

This dialog box is used to sort, show/hide the columns displayed on the Memory Mapping Profiler panel.

If the display in the panel has been customized, all of those customizations can be returned to the default state in this dialog box.

Filter Settings dialog box

This dialog box is used to set filtering conditions for display of memory mapping information on the Memory Mapping Profiler panel or variable access information on the Functions and Variables Access Table panel.

Dependent Projects Settings dialog box

This dialog box is used to reference/set the dependent projects.

Smart Report dialog box

This dialog box is used to collectively output quality-related information such as a list of source files, build option settings, information on functions and variables, and coverage rates.

Link Order dialog box

This dialog box is used to refer object module files and library files to be input to the linker and configure these link orders.

Optimization Performance Comparison Tool dialog box

This dialog box is used to measure and compare the ROM size or execution speed for the case in which the build options recommended by the build tool are applied.

Build Mode Settings dialog box

This dialog box is used to add and delete build modes and configure the current build mode in batch.

Batch Build dialog box

This dialog box is used to do build, rebuild and clean process in batch with the build mode that the project has.

Progress Status dialog box

This dialog box is used to display how the process has been progressed when the time consuming process is taken place.

Message dialog box

This dialog box is used to display messages output by the various tools.

Pack Settings dialog box

This dialog box is used to pack and save the project and this product.

Option dialog box

This dialog box is used to configure the CS+ environment.

Plug-in Manager dialog box

This dialog box is used to set the plug-ins to be read in when this product is started.

User Setting dialog box

This dialog box allows you to customize toolbars and menus displayed in the Main window.

New Toolbar dialog box

This dialog box is used to create a new toolbar to appear in the Main window.

Rename Toolbar dialog box

This dialog box is used to edit the name of a toolbar created by the user.

Customize Keyboard dialog box

This dialog box is used to assign shortcut keys to the various commands.

Rearrange Commands dialog box

This dialog box allows you to change the arrangement (including addition and deletion) of menu items and buttons in the Main window.

Other Windows... dialog box

This dialog box is used to select one of the divide panels shown in the Main window to activate or close.

Version Information dialog box

This dialog box is used to display versions of CS+ and each plug-in product.

Detail Version Information dialog box

This dialog box is used to display detail version information of this product and the present project information.

One Point Advice dialog box

This dialog box is used to display tips for using CS+.