Detailed Settings of Point Trace dialog box [Full-spec emulator][E1][E20]


This dialog box is used to display and change the detailed information on the point trace event selected on the Events panel. For details on point trace event setting, see "2.12 Collect Execution History of Programs".

Figure A.47

Detailed Settings of Point Trace Dialog Box [Full-spec emulator][E1][E20]

 

This section describes the following.

[How to open]

-

On the Events panel, move the caret to the point trace event of which you wish to change the detailed information, then select [Edit Condition...] from the context menu.

[Description of each area]

(1)

Detailed information display/change area

In this area, detailed information on the point trace event selected in the Events panel is displayed by category in the list. Also, you can directly change its settings.

(2)

Property description area

In this area, brief description of the categories and properties selected in the detailed information display/change area is displayed.

[Toolbar]

 

Displays categories in the detailed information display/change area.

 

Hides categories in the detailed information display/change area and rearranges only property items in the ascending order.

[Description of each category]

(1)

[Address condition]

You can display and modify the address condition of the point trace.

Start address

Specify the start address.

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

Address expression within the valid range

End address

Specify the end address.

Default

The current set value

Modifying

Directly enter from the keyboard.

Available values

Address expression within the valid range

(2)

[Target]

You can display and modify the target of the point trace.

Event target

Specify the target of the point trace.

Default

CPU

Modifying

Select from the drop-down list.

Available values

One of the following as selected from the drop-down list.

CPU, Global RAM

[Function buttons]

Button

Function

OK

Applies the detailed settings specified in the dialog box to the timer event and closes this dialog box.

Cancel

Nullifies settings and closes this dialog box.

Help

Displays the help for this dialog box.