Property panel


This panel is used to display and set the debug tool operation environment that is selected in the Project Tree panel.

Figure A.5

Property Panel (When E1 Is Selected)

 

This section describes the following.

[How to open]

-

On the Project Tree panel, select the [Microcontroller type Debug tool name (Debug Tool)] node to use, and then select [Property] from the [View] menu or the context menu.

-

On the Project Tree panel, double-click the [Microcontroller type Debug tool name (Debug Tool)] node to use.

Remark

If this panel has been opened, the detailed information on the debug tool is displayed by selecting the [Microcontroller type Debug tool name (Debug Tool)] node on the Project Tree panel.

[Description of each area]

(1)

Detailed information display/change area

In this area, the detailed information on the debug tool that is selected in Project Tree panel is displayed by category in the list. Also, you can directly change its settings.

The mark is indicates all the items in the category are expanded. The mark indicates all the items are collapsed. You can expand/collapse the items by clicking these marks or double-clicking the category name.

Note that only the hexadecimal number is allowed in the text box if the mark is displayed in the property configuration area.

For details on the information/how to setup in the category and property items contained in it, see the section explaining the corresponding tab.

(2)

Tab selection area

Categories for the display of the detailed information are changed when each tab is selected.

In this panel, following tabs are contained (see the section explaining each tab for details on the display/setting on the tab).

 

[[Edit] menu (Property panel-dedicated items)]

Undo

Undoes the latest property value editing being done.

Cut

Deletes the selected character string(s) and copies them to the clipboard while editing the property value.

Copy

Copies the contents of the selected range to the clipboard as character string(s).

Paste

Pastes the contents of the clipboard to the property value while editing the property value.

Delete

Deletes the selected character string(s) while editing the property value.

Select All

Selects all the character strings in the selected property while editing the property value.

Find...

Opens the Find and Replace dialog box with selecting [Quick Find] tab.

[Context menu]

[While not editing the property value]

Reset to Default

Restores the selected setting of the property item to default value.

Reset All to Default

Restores all the selected settings of the property items on the tab to default value.

 

[While editing the property value]

Undo

Undoes the latest property value editing being done.

Cut

Deletes the selected character string(s) and copies them to the clipboard while editing the property value.

Copy

Copies the contents of the selected range to the clipboard as character string(s).

Paste

Pastes the contents of the clipboard to the property value while editing the property value.

Delete

Deletes the selected character string(s) while editing the property value.

Select All

Selects all the character strings in the selected property while editing the property value.