A.1 Description

The table below lists the windows, panels and dialog boxes associated with debugging.

Table A.1

List of Window, Panel and Dialog Box

Window, panel and dialog-box names

Functional description

Main window

Controls program execution and opens each panel.

Project Tree panel

Selects the debug tool to be used.

Property panel

Displays detailed information on a debug tool selected on the Project Tree panel and changes settings.

Memory panel

Displays memory values and changes values.

Disassemble panel

Displays disassembled result of memory values and performs line assembly and instruction-level debugging.

CPU Register panel

Displays contents of CPU registers (program and system registers) and changes values.

IOR panel

Displays contents of I/O registers and changes values.

Local Variables panel

Displays contents of local variables and changes values.

Watch panel

Displays contents of registered watch-expressions and changes values.

Call Stack panel

Displays information on call stack used in function calls.

Trace panel

Displays trace data acquired from the debug tool.

Events panel

Displays detailed information on set events, chooses to enable or disable events, and deletes events.

Output panel

Displays messages output by the build tool, debug tool or each plug-in, or displays result of global search performed in Find and Replace dialog box.

Debug Console panel

Performs standard I/O.

Memory Mapping dialog box

Sets memory mapping.

Download Files dialog box

Selects a file to be downloaded and sets download condition.

Action Events dialog box

Sets action events.

Column Number Settings dialog box

Sets the number of view columns of memory values on the Memory panel.

Address Offset Settings dialog box

Sets an offset value for the address display on the Memory panel.

Memory Initialize dialog box

Initializes memory.

Memory Search dialog box

Searches memory.

Print Address Range Settings dialog box

Sets a print range on the Disassemble panel.

Trace Search dialog box

Searches for trace data.

Combination Condition dialog box [E1][E20] [EZ Emulator]

Displays the conditions for event combination and modifies the settings.

Detailed Settings of Timer Measurement dialog box [E1] [E20] [EZ Emulator]

Displays the detailed information on timer events and modifies the settings.

Detailed Settings of Execution Events dialog box

Displays the detailed information on execution-related events and modifies the settings.

Detailed Settings of Access Events dialog box

Displays the detailed information on access-related events and modifies the settings.

Detailed Settings of Interrupt Events dialog box [Simulator]

Displays the detailed information on interrupt events and modifies the settings.

Port Setting dialog box

Sets COM port in the Debug Console panel.

Scroll Range Settings dialog box

Sets a scroll range on the Memory panel/Disassemble panel.

Go to the Location dialog box

Moves the caret to a specified position.

Data Save dialog box

Saves displayed content of each panel and upload data.

Functions and Variables Access Table panel

Displays the functions that access variables in the form of an orthogonal table.