R_DAC_Change_OutputVoltage_8bit


Changes the output voltage of D/A converter.(8bit mode)

[Syntax]

#include    "r_cg_macrodriver.h"
void    R_DAC_Change_OutputVoltage_8bit ( uint8_t outputVoltage );

[Argument(s)]

I/O

Argument

Description

I

uint8_t outputVoltage;

output Voltage (Low 8bit)

[Return value]

None.