R_DAC_Change_OutputVoltage


Changes the output voltage of D/A converter.(12bit mode)

[Syntax]

#include    "r_cg_macrodriver.h"
void    R_DAC_Change_OutputVoltage ( uint16_t outputVoltage );

[Argument(s)]

I/O

Argument

Description

I

uint16_t outputVoltage;

output Voltage (Low 12bit)

[Return value]

None.