R_IICAn_Set_PowerOff


Halts the clock supplied to the serial interface IICA.

Remark

Calling this API function changes the serial interface IICA to reset status.
For this reason, writes to the control registers (e.g. IICA control register n: IICCTLn) after this API function is called are ignored.

[Syntax]

void    R_IICAn_Set_PowerOff ( void );

Remark

n is the channel number.

[Argument(s)]

None.

[Return value]

None.