r_iican_callback_slave_error


Performs processing in response to detection of IICA slave communication error.

[Syntax]

#include    "r_cg_macrodriver.h"
static  void    r_iican_callback_slave_error ( MD_STATUS flag  );

Remark

n is the channel number.

[Argument(s)]

I/O

Argument

Description

I

MD_STATUS flag;

Cause of communication error

MD_ERROR: Address mismatch detected

MD_NACK: Acknowledge not detected
(Master receiving end)

[Return value]

None.