r_mac32bit_interrupt_flow


Performs processing in response to the 32-bit Multiply-accumulator interrupt INTMACLOF.

Remark

This API function is called as the interrupt process corresponding to the 32-bit Multiply-accumulator interrupt INTMACLOF.

[Syntax]

CA78K0R Compiler

__interrupt static  void    r_mac32bit_interrupt_flow ( void );

 

CC-RL Compiler

static  void  __near r_mac32bit_interrupt_flow ( void );

[Argument(s)]

None.

[Return value]

None.