3.2.46 32-bit Multiply-accumulator

Below is a list of API functions output by the Code Generator for 32-bit Multiply-accumulator use.

Table 3.46

API Functions: [32-bit Multiply-accumulator]

API Function Name

Function

R_MAC32Bit_Create

Performs initialization necessary to control the data operation circuit.

R_MAC32Bit_Create_UserInit

Performs user-defined initialization related to the data operation circuit.

r_mac32bit_interrupt_flow

Performs processing in response to the DOC operation result detection interrupt INTDOC.

R_MAC32Bit_Reset

Gets result of addition or subtraction.

R_MAC32Bit_Set_PowerOff

Clears DOPCF flag of DOC control register (DOCR).

R_MAC32bit_MULUnsigned

Operates the unsigned multiply.

R_MAC32Bit_MULSigned

Operates the signed multiply.

R_MAC32Bit_MACUnsigned

Operates the unsigned multiply-accumulate.

R_MAC32Bit_MACSigned

Operates the signed multiply-accumulate.