r_iicmn_interrupt


Performs processing in response to the simple IIC communication end interrupt INTIICmn.

Remark

This API function is called as the interrupt process corresponding to the simple IIC communication end interrupt INTIICmn.

[Syntax]

__interrupt static  void    r_iicmn_interrupt ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.