r_iicmn_callback_master_error


Performs processing in response to detection of parity error (ACK error).

[Syntax]

#include    "r_cg_macrodriver.h"
static  void    r_iicmn_callback_master_error ( MD_STATUS flag );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

I/O

Argument

Description

O

MD_STATUS flag;

Cause of communication error

MD_NACK: Acknowledge not detected

[Return value]

None.