R_TAUm_Channeln_Start


Starts the count for channel n.

Remark

The time from the call to this API function to the start of counting depends on the type of the function in question (e.g. interval timer, square-wave output, or external event counter).

[Syntax]

void    R_TAUm_Channeln_Start ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.