R_TAUm_Set_PowerOff


Halts the clock supplied to the timer array unit.

Remark

Calling this API function changes the timer array unit to reset status.
For this reason, writes to the control registers after this API function is called are ignored.

[Syntax]

void    R_TAUm_Set_PowerOff ( void );

Remark

m is the unit number.

[Argument(s)]

None.

[Return value]

None.