R_TMR_KBm_Create_UserInit


Performs user-defined initialization relating to the 16-bit timer KB.

Remark

This API function is called as the R_TMR_KB_Create callback routine.

[Syntax]

void    R_TMR_KBm_Create_UserInit ( void );

Remark

m is the unit number.

[Argument(s)]

None.

[Return value]

None.