R_TMR_KBmn_ForcedOutput_Start


Enables input of the trigger signal used for the forced output stop function.

[Syntax]

void    R_TMR_KBmn_ForcedOutput_Start ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.