R_KB2m_TKBOn1_DitheringFunction_Start


Starts dithering function for timer output TKBOn1.

[Syntax]

void    R_KB2m_TKBOn1_DitheringFunction_Start ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.