R_KB2m_TKBOn0_SmoothStartFunction_Stop


Ends smooth start function for timer output TKBOn0.

[Syntax]

void    R_KB2m_TKBOn0_SmoothStartFunction_Stop ( void );

Remark

m is the unit number, and n is the channel number.

[Argument(s)]

None.

[Return value]

None.